Note:
The Processor SDK Linux image provides
an interactive user demo by default. Once booted, the board acts as a Wireless
access point with SSID AM64xSK-AP and Password tiwilink8. Once
connected, the demo can be found by navigating to http://192.168.43.1:8081. More details can be found on the Software
Quick Start Guide, located on the product page.
- Place the SK EVM boot switch
selectors (SW2, SW3) into selected boot mode. Example boot-modes for SD card and
no-boot are shown below. For additional options, see Section 4.4.4.1.
- Connect your boot media (if
applicable).
- Attach the 5 V USB Type-C cable to
the SK EVM Type-C (J8) Connector.
- Connect the other end of the Type-C
cable to the source, either AC Power Adapter, or Type C source device (such as a
Laptop computer).
- Use ON/OFF sliding switch SW5 to
Power on the board.
- Visually inspect the LEDs against the
reference photos below. The following LEDs are illuminated: LD2 and LD16 on top side
of the board.
- XDS110 JTAG and UART debug console
output are routed to micro-USB ports J12 and J11, respectively.
Note: Linux console output is routed to
the second enumerated ttyUSB port.