SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
Table 26-4 details the Beckhoff ®Automation errata of the EtherCAT IP integrated onto this device.
Errata Number | Description |
---|---|
ER#156 | WKC increment for reading reserved FMMU registers (+0xD-+0xF) |
ER#158 | WKC increment for writing 0x0914-0x0917 |
ER#162 | ESC DL Control (0x0101) loop setting Auto-Close (01): if port waits for write access to be opened, the temporary loop bit (0x0100[1]) is not taken into account when a write command to ESC DL Control occurs. |
ER#164 | EEPROM FSM cannot accept another command within 1680 ns after finishing a previous command |
ER#165 | EtherCAT reset register 0x0040 cannot be written using VLAN tagged frames, because state is reset due to double ECAT_CLEAR. VLAN tagged frames are rarely used for EtherCAT. |
ER#168 | Changing SyncSignal cycle times during activation can lead to extremely long cycle times, resulting from (intermediate) violation of the minimum delay between two consecutive pulses. For example, changing Sync1 from a few ns before Sync0 to a few ns after Sync0 results in a missed Sync1 time, which can take up to several 32/64-bit turn-arounds until the next pulse occurs. Changing cycle time from PDI can result in usage of intermediate, inconsistent values, which can result in unwanted cycle times or extremely long delays as above. |