SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
FILE: bgcrc_ex1_cpuinterrupt.c
This example demonstrates how to configure and trigger BGCRC from the CPU. BGCRC module is configured for 1 KB of GS0 RAM which is programmed with a known data. The pre-computed CRC value is used as the golden CRC value. Interrupt is generated once the computation is done and checks if no error flags are raised Calculation uses the 32-bit polynomial 0x04C11DB7 and seed value 0x00000000.
External Connections
Watch Variables