SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
This chapter describes the enhanced capture (eCAP) module and the high resolution capture (HRCAP) module, which are used in systems where accurate timing of external events is important.
The enhanced capture (eCAP) module is a Type 3 eCAP.
The high resolution capture (HRCAP) module is part of the eCAP module. HRCAP measures the width of external pulses to a higher degree of accuracy than the eCAP module.
See the C2000 Real-Time Control Peripheral Reference Guide for a list of all devices with an eCAP and HRCAP module of the same type, to determine the differences between the types, and for a list of device-specific differences within a type. A detailed description of all referenced functions can be found in the C2000Ware documentation.