SPRUIZ1B July 2023 – August 2024 TMS320F28P650DH , TMS320F28P650DK , TMS320F28P650SH , TMS320F28P650SK , TMS320F28P659DH-Q1 , TMS320F28P659DK-Q1 , TMS320F28P659SH-Q1
The PWM Sync-chain on the MCU can be triggered either by the device external inputs from the GPIO via input cross-bar or the PWM internal events when the chain is programmed appropriately. The SYNC0/1 inputs in this implementation also act as the external sync inputs to the PWM sync-chain. The integration is shown in Figure 26-18.
The additional select register added to the trigger crossbar register allows independent programming of the EXTSYNCx from either GPTRIP or SYNC0/1.