The F280039C controlCARD (TMDSCNCD280039C) from Texas Instruments (TI) provides a great way to learn and experiment with F28003x devices. The F28003x devices are members of TI’s C2000™ family of microcontrollers (MCUs). This 120-pin controlCARD is intended to provide a well-filtered robust design that is capable of working in most environments. This document provides the hardware details of the F280039C controlCARD and explains the functions, locations of jumpers, and connectors present on the board.
C2000™ and Code Composer Studio™ are trademarks of Texas Instruments.
All trademarks are the property of their respective owners.
Each controlCARD comes with a Hardware Developer’s Kit, which is a full set of files necessary to evaluate and develop with a C2000 device. These files include:
The Hardware Developer's Kit for the controlCARD can be found in the C2000Ware at the following location:
The controlCARD can be completely powered and operated from the USB-C connector. In this stand-alone mode the on-board isolated power supply will provide power to the F280039C device; no additional hardware is required. Optionally, an external 5-V supply can be provided to power the F280039C device. For a detailed explanation of the hardware configuration, see Section 4.3.
When the controlCARD is used in a high-voltage setup, it is the user’s responsibility to confirm that the voltages and isolation requirements are identified and understood prior to energizing the board or simulation. When energized, the controlCARD or components connected to the controlCARD should not be touched. Furthermore, the capacitor C7:A should be removed to minimize the possibility of leakage current flowing across the isolation barrier of the controlCARD.
Configuration 1: Stand-alone
Configuration 2: External 5-V supply
The TMDSCNCD280039C controlCARD automatically switches to the external 5-V supply when present. No additional configuration is required.
Current revision of controlCARD as of 5/3/2021: PCB rev - E1, ASSY rev - none.
5-V power suppy instabilty may lead to device resets
The 5-V rail on the TMDSCNCD280039C controlCARD can be powered from an on-board USB connector or from a baseboard like the TMDSHSECDOCK. A switch device on the controlCARD automatically selects the 5-V input power source for the controlCARD without the need for user configuration.
A loss of power or glitching on the baseboard 5-V power source can cause the automatic switch to disconnect from both power sources for several milliseconds. This momentary loss of power may cause a brownout condition on the MCU, triggering a device reset. To avoid this condition, ensure that the baseboard power supply remains at 0 V or 5 V during code execution.