Note: The AM243x LaunchPad requires a
5 V, 3A power supply in order to function. While a USB type-C cable is included,
A 5 V, 3A power supply is
not included in the kit and must be ordered
separately. The
Belkin USB-C Wall Charger is known to work
with the LaunchPad and the supplied type-C cable. For more information on power
requirements go to
Section 3.1. If there is an error in the power input then the red LED (LD9) will glow
continuously. For more information about the power status LED's, see
Section 3.1.2.
Note: The JTAG connection through the
micro-B USB port needs to be made after power is supplied to the LaunchPad by
the USB type-C connection. The JTAG may not connect if the micro-B USB
connection is made before the 5 V, 3A connection is made. For more information
on JTAG emulation go to
Section 4.15 .
Note: For E1 and E2 revisions of the
AM243x LaunchPad, some output signals are not able to propagate to the
BoosterPack headers. Any pinmux configuration that is an output signal for balls
R21, T19, U18, U20, V20 of the SoC will be gated by the isolation buffer U32
because the DIR pin of the buffer is low (only allowing data transfer from side
B to A). The signals that not able to propagate to the BoosterPack headers
include: UART2_RTSn, EHRPWM2_A, EHRPWM2_B, as well as any GPIO signals on the
listed pins.