SPRUJ12F August 2021 – January 2024 AM2431 , AM2432 , AM2434
The AM243x LaunchPad may have a Non-Secure (GP or General Purpose) or a Secure device (HS-FS). To determine if the device is secure, refer to field parameter for device revision: "r" of the Device name. If the Device Revision is "B" or a subsequent alphabetical letter, then the device is a Secure device.
A Secure device has the ability to use a one time programming to convert the device from High Security Field Securable (HS-FS) to High Security Security Enforced (HS-SE).
A secure device leaves the TI factory in an HS-FS state where customer keys are not programmed and has the following attributes:
The One Time Programmable (OTP) keywriter converts the secure device from HS-FS to HS-SE. The OTP keywriter programs customer keys into the device eFuses to enforce secure boot and establish a root of trust. The secure boot requires an image to be encrypted (optional) and signed using customer keys, which will be verified by the SoC. A secure device in the HS-SE state has the following attributes: