SPRUJ12F August 2021 – January 2024 AM2431 , AM2432 , AM2434
Figure 4-5 shows the reset architecture of the AM243x LaunchPad.
The SoC has the following resets:
Three push button switches are available to provide reset for MCU_PORz, MCU_RESETz and RESET_REQz as seen in Section 3.2.
MCU_PORz signal is provided by the outputs of a voltage monitor IC (TPS386000RGPR) for the core and peripheral voltages where the enable of this voltage monitor is controlled by the PORz signal from the test automation header or push button switch (SW1).
MCU domain warm reset (MCU_RESETz) is provided from a push button switch (SW2)
Main domain warm reset (SoC_RESET_REQz) is provided by the Warm Reset signal from the test automation header or a push button switch (SW3).
Upon Power on Reset, all peripheral devices connected to MCU domain get reset by MCU_RESETSTATz.
One User input interrupt is connected to one of the GPIO of SoC.