SPRUJ12F August 2021 – January 2024 AM2431 , AM2432 , AM2434
The following sequence should be followed for proper functioning of JTAG:
The AM243x LaunchPad includes the necessary circuitry for XDS110 emulation. The XDS110 class on-board emulation is used to support testing of software builds. The connection for the emulator uses a USB 2.0 micro-B connection (J20) and the circuit acts as a powered USB peripheral device. The VBUS power from the connector is used to power the emulation circuit such that the connection to the emulator is not lost when power to the LaunchPad is removed. Voltage translation buffers are used to isolate the XDS110 circuit from the rest of the LaunchPad.
An ESD protection diode (TPDE02B04DQAR) is provided on the USB signals to steer ESD current pulses to VCC or GND. The ESD protection diode protects against ESD pulses up to ±2.5 kV Human-Body Model (HBM) as specified in ANSI/ESDA/JEDEC JS-001 and provides ±12 kV contact discharge as well as ±15 kV air-gap discharge as specified in IEC 61000-4-2.