The Industrial application LEDs
consist of five green, one red, and two bi-color LEDs.
- Four green LEDs are connected
to the I2C-based LED driver (TPIC2810D) at the address 0x60 that is
controlled by the SoC at the SoC_I2C0 port. These LEDs are to be toggled
based on the Industrial application.
- The other green LED, as well
as the red and two bi-color LEDs, are connected to SoC GPIO's such that they
can be toggled based on the application.