The following requirements must be met when operating the AWR2944EVM in the EU and UK.
- The tested operating bandwidths for Radio
Equipment Directive 2014/53/EU and UKCA compliance are 900MHz (77.45GHz center
frequency) and 3900MHz (78.95GHz center frequency). The maximum peak EIRP is
approximately 37dBm for the 900MHz bandwidth and 34dBm for the 3900MHz
bandwidth.
- If users choose to
operate the EVM outside of the specified operating bandwidth and
operating power as described above, then the EVM must be operated inside
a shielded chamber.
- When operating in the 77GHz to 81GHz region,
users must not enable more than one simultaneous TX for 0dB backoff or enable a
minimum of 10dB TX backoff for multiple simultaneous TX to meet the -3 dBm limit
for mean power spectral density.
- The automotive Ethernet PHY (U4) and port (J4) on
the AWR2944EVM have not been tested by Texas Instruments to be compliant with
any regional standards such as Radio Equipment Directive 2014/53/EU. If users
wish to populate the components necessary to utilize this port, then users can
do any necessary testing to verify that the port is compliant with all
applicable regional standards before use. Any modifications done to enable the
J4 port invalidate the existing RED 2014/53/EU certification of the
AWR2944EVM.
- The RJ45 port (J9) has been tested to be
compliant with the Radio Equipment Directive 2014/53/EU and UKCA requirements
using an unshielded, symmetrical indoor CAT5 or higher Ethernet cable with a
maximum length of 3 meters. If users wish to operate the AWR2944EVM with an
Ethernet cable that does not meet these specifications, then users can do any
necessary testing to verify that the AWR2944EVM and Ethernet cable is compliant
with all applicable regional standards before use.
- The AWR2944EVM has been tested to be compliant
with the Radio Equipment Directive 2014/53/EU and UKCA requirements using a DC
power cable with a maximum length of 3 meters. If users wish to operate the
AWR2944EVM with a longer DC power cable length, then users can do any necessary
testing to verify that the AWR2944EVM and DC power cable is compliant with all
applicable regional standards before use.
- The AWR2944EVM has been tested to be compliant
with the Radio Equipment Directive 2014/53/EU and UKCA requirements using a USB
cable with a maximum length of 3 meters. If users wish to operate the AWR2944EVM
with a longer USB cable length, then users can do any necessary testing to
verify that the AWR2944EVM and USB cable is compliant with all applicable
regional standards before use.