Download and install C2000WARE-MOTORCONTROL-SDK software package from the link provided by TI, install this Motor Control SDK software in its default folder. C2000WARE-MOTORCONTROL-SDK can be installed in one of two ways:
Go to CCS and under View → Resource Explorer. Under the TI Resource Explorer, go to Software→C2000Ware_MotorControl_SDK, and click on the install button.
Once the installation is complete, close CCS, and create a new workspace for importing the project. The software project of this example lab is inside the C2000Ware Motor Control SDK folder at <install_location>\C2000Ware_MotorControl_SDK_<version>\solutions\universal_motorcontrol_lab. Follow these steps to build and run this code with different incremental builds as described in the following sections.