SPRUJ26A September 2021 – April 2024
If using a custom board, make sure that the power supply to the C2000 microcontroller and to the gate driver is correct, and that the JTAG emulator can be connected successfully. Modify the reference code to be compatible with the custom board as described in the following sections, and then run the code starting with build level 1 and working the way to build level 4 as illustrated in Section 3.5.