SPRUJ26A September 2021 – April 2024
Table 3-3 shows the various connections available on the board. The location of these connections on the board are shown in Figure 3-17.
[Main]-P1 | AC input connector (110V – 220V AC) |
[Main]-TB3 | Terminal Block to connect motor |
[Main]-BS1 | Banana Jack for Output from AC Rectifier |
[Main]-BS2, BS6 | Banana Jack for GND Connection |
[Main]-BS3 | Banana Jack for connecting an input voltage for the PFC stage, this would typically be rectified AC voltage from the [Main]-BS1 connector. |
[Main]-BS4 | Banana Jack for connecting a load to the output from the PFC stage, When using PFC+Motor project the output of the PFC stage would connect to the input for the inverter bus i.e. [Main]-BS5 |
[Main]-BS5 | Banana Jack for input of DC bus voltage for the inverter |
[Main]-J2 | Aux power supply module
input voltage selection jumper,
|
[Main]-J3, J4, J5 | Jumpers J3,J4 and J5 are used for sourcing 15V, 5V and 3.3V power respectively for the board from the 15V DC Power supply. |
[Main]-J7 | J7 is used to select the over current protection threshold source |
[Main]-J8 | J8 is used to enable/disable the IPM over current protection |
[Main]-J9 | JTAG TRSTn disconnect jumper, populating the jumper enables JTAG connection to the Microcontroller. The jumpers need to be unpopulated when no JTAG connection is required such as when booting from FLASH. |
[Main]-J14 | PWMDAC outputs: Gives voltage outputs that result from a PWM being attached to a first-order low-pass filter. Pins 1,2,3 and 4 are attached to low pass filtered PWM output pins respectively to observe system variables on an oscilloscope. |
[Main]-J16 | Isolated CAN bus connector |
[Main]-J17 | Connector to supply power to the DC fan (shipped with the board) that is attached to the IPM heat sink. |
[Main]-H1 | QEP connector: connects
with a 0-5V QEP sensor to gather information on a motor’s speed and
position. CAP/Hall effect sensor connector: connects with a 0-5V sensor to gather information on a motor’s speed and position. |
[M1]-F1 | Fuse for the AC input |
[M3]-JP1 | USB connection for on-board emulation |
[M3]-J2 | External JTAG interface: this connector gives access to the JTAG emulation pins. If external emulation is desired, place a jumper across [M3]-J5 and connect the emulator to the board. To power the emulation logic a USB connector will still need to be connected to [M3]-JP1. |
[M3]-J5 | On-board emulation disable jumper: Place a jumper here to disable the on-board emulator and give access to the external interface. |