SPRUJ27C November   2022  – November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1

 

  1.   1
  2.   Trademarks
  3. 1Introduction
    1. 1.1 Reference Material
    2. 1.2 Function Listing Format
  4. 2TMS320F28003x Flash API Overview
    1. 2.1 Introduction
    2. 2.2 API Overview
    3. 2.3 Using API
      1. 2.3.1 Initialization Flow
        1. 2.3.1.1 After Device Power Up
        2. 2.3.1.2 FMC and Bank Setup
        3. 2.3.1.3 On System Frequency Change
      2. 2.3.2 Building With the API
        1. 2.3.2.1 Object Library Files
        2. 2.3.2.2 Distribution Files
      3. 2.3.3 Key Facts For Flash API Usage
  5. 3API Functions
    1. 3.1 Initialization Functions
      1. 3.1.1 Fapi_initializeAPI()
    2. 3.2 Flash State Machine Functions
      1. 3.2.1 Fapi_setActiveFlashBank()
      2. 3.2.2 Fapi_issueAsyncCommandWithAddress()
      3. 3.2.3 Fapi_issueBankEraseCommand()
      4. 3.2.4 Fapi_issueProgrammingCommand()
      5. 3.2.5 Fapi_issueProgrammingCommandForEccAddresses()
      6. 3.2.6 Fapi_issueFsmSuspendCommand()
      7. 3.2.7 Fapi_issueAsyncCommand()
      8. 3.2.8 Fapi_checkFsmForReady()
      9. 3.2.9 Fapi_getFsmStatus()
    3. 3.3 Read Functions
      1. 3.3.1 Fapi_doBlankCheck()
      2. 3.3.2 Fapi_doVerify()
      3. 3.3.3 Fapi_calculatePsa()
      4. 3.3.4 Fapi_doPsaVerify()
    4. 3.4 Informational Functions
      1. 3.4.1 Fapi_getLibraryInfo()
    5. 3.5 Utility Functions
      1. 3.5.1 Fapi_flushPipeline()
      2. 3.5.2 Fapi_calculateEcc()
      3. 3.5.3 Fapi_isAddressEcc()
      4. 3.5.4 Fapi_remapEccAddress()
      5. 3.5.5 Fapi_calculateFletcherChecksum()
  6. 4Recommended FSM Flows
    1. 4.1 New Devices From Factory
    2. 4.2 Recommended Erase Flow
    3. 4.3 Recommended Bank Erase Flow
    4. 4.4 Recommended Program Flow
  7. 5Software Application Assumptions of Use Related to Safety
  8.   A Flash State Machine Commands
    1.     A.1 Flash State Machine Commands
  9.   B Compiler Version and Build Settings
  10.   C Object Library Function Information
    1.     C.1 TMS320F28003x Flash API Library
  11.   D Typedefs, Defines, Enumerations and Structures
    1.     D.1 Type Definitions
    2.     D.2 Defines
    3.     D.3 Enumerations
      1.      D.3.1 Fapi_FlashProgrammingCommandsType
      2.      D.3.2 Fapi_FlashBankType
      3.      D.3.3 Fapi_FlashStateCommandsType
      4.      D.3.4 Fapi_FlashReadMarginModeType
      5.      D.3.5 Fapi_StatusType
      6.      D.3.6 Fapi_ApiProductionStatusType
    4.     D.4 Structures
      1.      D.4.1 Fapi_FlashStatusWordType
      2.      D.4.2 Fapi_LibraryInfoType
  12.   E Parallel Signature Analysis (PSA) Algorithm
    1.     E.1 Function Details
  13.   F ECC Calculation Algorithm
    1.     F.1 Function Details
  14.   G Errata
  15.   Revision History

Errata

Advisory 1:

  • Incorrect Revision number returned by the Fapi_getLibraryInfo() of FAPI_F28003x_EABI_v1.58.10.lib

Flash API Version affected:

  • FAPI_F28003x_EABI_v1.58.10.lib.

Details:

  • Fapi_getLibraryInfo() is incorrectly coded to return the Revision number value as 01 instead of 10. If the application does not use this function, then this advisory is not applicable.

WorkAround:

  • User application should treat 01 as 10.

Advisory 2:

  • DCSM OTP programming is not supported by the FAPI_F28003x_EABI_v1.58.10.lib for F280033/34 devices. This advisory is not applicable for non-F280033/34 devices.

Flash API Version affected:

  • FAPI_F28003x_EABI_v1.58.10.lib.

Details:

  • FlashAPI programming command is blocking the programming of DCSM OTP range. If the F280033/34 user application does not program the DCSM OTP, then this advisory is not applicable.

WorkAround:

  • If the F280033/34 user application needs to program DCSM OTP, then FAPI_F280033_34_EABI_v1.58.11.lib should be used. Non-F280033/34 users should continue to use the FAPI_F28003x_EABI_v1.58.10.lib.