SPRUJ27C November 2022 – November 2023 TMS320F280033 , TMS320F280034 , TMS320F280034-Q1 , TMS320F280036-Q1 , TMS320F280036C-Q1 , TMS320F280037 , TMS320F280037-Q1 , TMS320F280037C , TMS320F280037C-Q1 , TMS320F280038-Q1 , TMS320F280038C-Q1 , TMS320F280039 , TMS320F280039-Q1 , TMS320F280039C , TMS320F280039C-Q1
Verifies region specified is erased value
Synopsis
Fapi_StatusType Fapi_doBlankCheck(
uint32 *pu32StartAddress,
uint32 u32Length,
Fapi_FlashStatusWordType *poFlashStatusWord)
Parameters
pu32StartAddress [in] | Start address for region to blank check | |
u32Length [in] | Length of region in 32-bit words to blank check | |
poFlashStatusWord [out] | Returns the status of the operation if result is not Fapi_Status_Success | |
->au32StatusWord[0] | Address of first non-blank location | |
->au32StatusWord[1] | Data read at first non-blank location | |
->au32StatusWord[2] | Value of compare data (always 0xFFFFFFFF) | |
->au32StatusWord[3] | N/A |
Description
This function checks if the flash is blank (erased state) starting at the specified address for the length of 32-bit words specified. If a non-blank location is found, corresponding address and data will be returned in the poFlashStatusWord parameter.
Restrictions
None
Return Value