SPRUJ28E November 2021 – September 2024 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The Host driver writes the boot timeout value as per the eMMC4.3+ spec into MMCSD0_BOOT_TIMEOUT_CONTROL register.
If the "ALT_BOOT_MODE" and "BOOT_ENABLE" is set to 1 in MMCSD0_BLOCK_GAP_CONTROL register and "DATA_XFER_DIR" bit is set to 1 in MMCSD0_TRANSFER_MODE register, the host controller drives the CMD0 (0xFFFFFFFA) on the CMD line.
The system shall wait for command complete interrupt before "RCV_BOOT_ACK" interrupt (MMCSD0_NORMAL_INTR_STS[13] RCV_BOOT_ACK).
If the Host controller is configured to wait for boot acknowledgement from the eMMC4.3+ device, the controller receives the boot acknowledgement and asserts the "RCV_BOOT_ACK" interrupt to the driver.
The eMMC4.3+ device starts sending the boot data on the data line and Host controller sends the same to system whenever a block of data is received from device. The System needs to send CMD0 to inform the device about the boot operation complete. The system shall program MMCSD0_COMMAND register with argument "00000000h" for the CMD0 and waits for command complete.
The Host controller terminates the boot operation when the programmed number of blocks are transferred to the System and the Driver shall send CMD0 to eMMC card and then program "BOOT_ENABLE" as "0" in MMCSD0_BLOCK_GAP_CONTROL register.
The boot operation can be terminated at any time (the Driver can send CMD0 and set the "BOOT_ENABLE" as "0" anytime to disable the boot operation). After the boot termination, all state machines in the Host controller need to move to IDLE state. The Host controller asserts the soft reset for CMD and data line internally when the driver clears the BOOT_COMPLETE interrupt (MMCSD0_NORMAL_INTR_STS[14] BOOT_COMPLETE) and all the state machine goes to the idle state.
If the Host controller doesn't receive the acknowledgement from the device with in timeout value the Host controller will assert the data timeout error interrupt (MCSD0_ERROR_INTR_STS[4] DATA_TIMEOUT).
The driver programs the MMCSD0_BOOT_TIMEOUT_CONTROL register with boot data timeout value.
There is no need to perform error recovery sequence in case of data timeout interrupt as mentioned above. If the device sends wrong acknowledgement to the Host, then Host controller will assert Data CRC Error interrupt to the Driver (MCSD0_ERROR_INTR_STS[5] DATA_CRC). The Host driver has to stop the boot mode operation by setting "ALT_BOOT_MODE" and "BOOT_ENABLE" as "0" in MMCSD0_BLOCK_GAP_CONTROL register and write soft reset for CMD and data line.
If the device sends end bit as "0" in acknowledgement to the Host, the Host controller asserts Data End Bit Error interrupt (MCSD0_ERROR_INTR_STS[6] DATA_ENDBIT) on the Driver. The Host driver stops the boot mode operation by setting "ALT_BOOT_MODE" and "BOOT_ENABLE" as "0" in MMCSD0_BLOCK_GAP_CONTROL register and write soft reset for CMD and data line.
Note: Enable the MMCSD0_BLOCK_GAP_CONTROL[7] BOOT_ACK_ENA bit during boot operation . If failed, the controller will not wait for boot acknowledge from the card and send out data CRC error when the card sends boot acknowledgement first and followed by boot data.