SPRUJ28E November 2021 – September 2024 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
Each memory is surrounded by an ECC wrapper which performs the ECC detection and correction. The wrapper communicates via serial interface with the aggregator which has memory a mapped configuration interface. For RAM wrapper types, after injecting the error, the RAM location where the error was injected needs to be accessed in order to trigger the error interrupt. If the “force_n_row” option is selected during error injection, then any RAM access will trigger the interrupt and the specific row is not needed.