POK monitoring occurs within the initial POK settling (from enable). It is
therefore required that the initial state of the POK after enable should be
discarded; further, the ESM should be configured for its system response after
the initial results during the settling time are discarded.
Within a PRG, all POKs must
ping-pong or all monitor a static threshold
It is not advised to change the threshold from UV to OV while the POK is
enabled