SPRUJ28E November 2021 – September 2024 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
Each proxy must have a single owner, as each proxy only has a single buffer to work on the current data. If there are multiple owners in the system, they must each use their own proxy. Then they will have their own buffer and each can access a different resource at the same time. Each proxy is completely independent and kept coherent regardless of accesses to other proxies or regardless of the order of accesses. So the proxies support interleaving of multiple hosts' accesses.