When an error event occurs, the user can query and collect the information about
the endpoint and offset information for the location relative to the start of
the associated RAM.
To clear the ECC error event, clear the pending status of the ECC error events
by configuring the ECC_RAM_ERR_STAT1 (for Wrapper type endpoints) and
SDL_EDC_CTL_ERR_STATUS1(for Interconnect type endpoints) register.
The ECC_SEC_EOI_REG register is used to re-trigger the pulse interrupt signal to
ensure that any nested interrupt events are serviced. The software interrupt
handler must write to the ECC_SEC_EOI_REG register at the end of the current
interrupt processing routine, so that new events can re-trigger the pulse
interrupt signal again. For level interrupt signals the ECC_SEC_EOI_REG register
is not functional and must not be used.
Clear the ESM error interrupt using the ESM registers.