SPRUJ28E November 2021 – September 2024 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
If the TLB lookup results in no matches and there is no chaining to another TLB (described later), then this is called a TLB miss. If the TLB misses, since there is no back-fill (such as from an MMU), the result is that the translation fails and will fault (a fault is when there is no physical address available). The transaction will be marked as in error with the flush signal, and a later slave will perform the flush that will return a bus error and read data as zeros. The PVU will record the fault as an interrupt and log the fault in the exception logging read-only registers.