SPRUJ28E November 2021 – September 2024 AM68 , AM68A , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VL-Q1
The Main domain instances of the RTI module are intended to function as a Digital Windowed Watchdog for the CPU core that they are associated with in Table 5-84. It is not intended to use an RTI that is provisioned for a particular CPU core with a different CPU core.
RTI Instance | Associated CPU |
---|---|
RTI0 | A72SS0_CORE0 |
RTI1 | A72SS0_CORE1 |
RTI2 | None. Use of this RTI is Reserved. |
RTI3 | None. Use of this RTI is Reserved. |
RTI4 | None. Use of this RTI is Reserved. |
RTI5 | None. Use of this RTI is Reserved. |
RTI6 | None. Use of this RTI is Reserved. |
RTI7 | None. Use of this RTI is Reserved. |
RTI15 | GPU |
RTI16 | C71SS_CORE0 |
RTI17 | C71SS_CORE1 |
RTI18 | None. Use of this RTI is Reserved. |
RTI19 | None. Use of this RTI is Reserved. |
RTI28 | R5FSS0_CORE0 |
RTI29 | R5FSS0_CORE1 |
RTI30 | R5FSS1_CORE0 |
RTI31 | R5FSS1_CORE1 |
RTI32 | None. Use of this RTI is Reserved. |
RTI33 | None. Use of this RTI is Reserved. |
The MCU_RTI Modules serve as a windowed watchdog for MCU_R5FSS0 as described in Table 5-85.
RTI Instance | Associated CPU |
---|---|
MCU_RTI0 |
MCU_R5FSS0 (Lockstep Mode) MCU_R5FSS0_CORE0 (Unlocked Mode) |
MCU_RTI1 | MCU_R5FSS0_CORE1 (Unlocked Mode) |