- Insert the TMDSCNCD2800157
controlCARD into a TMDSHSECDOCK, or other compatible docking station.
- Connect a USB cable to J17 on the
TMDSHSECDOCK.
- Flip S1 to the "USB-ON" position
on the TMDSHSECDOCK. The controlCARD automatically switches to the external 5-V
supply.
- LED1:A and D3 on the controlCARD
illuminate.
Note: The TMDSCNCD2800157 controlCARD
automatically switches to the external 5-V supply when present. No additional
configuration is required.