SPRUJ53B April 2024 – September 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
SYS_ERR consolidate several sources of interrupts (see Figure 3-3). These sources set the respective bit in the SYS_ERR_INT_FLG register. Any set bit in the SYS_ERR_INT_FLG register also sets the global interrupt (GINT) bit. The GINT bit has to be cleared before any SYS_ERR interrupt is generated. If the GINT bit is cleared with the source flags still set, another SYS_ERR interrupt is fired; therefore, it is recommended to clear the source flags before clearing the GINT bit.