SPRUJ53B April 2024 – September 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
This section describes the three 32-bit CPU timers (TIMER0/1/2) shown in Figure 3-12.
Timer0 and Timer1 can be used in user applications. Timer2 is reserved for real-time operating system uses (for example, TI-RTOS). If the application is not using an operating system that utilizes this timer, then Timer2 can be used in the application. timer interrupt signals (TINT0, TINT1, TINT2) are connected as shown in Figure 3-13.
The general operation of a CPU timer is as follows:
The registers listed in Section 3.16 are used to configure the timers.