SPRUJ59A April   2024  – September 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Feature Differences Between F28003x and F28P55x
    1. 1.1 F28003x and F28P55x Feature Comparison
  5. 2PCB Hardware Changes
    1. 2.1 PCB Hardware Changes for the 100-Pin PZ, 80-Pin PNA and 64-Pin PM Packages
    2. 2.2 100-Pin PZ, 80-Pin PNA and 64-Pin PM Migration Between F28003x and F28P55x For New and Existing PCB
    3. 2.3 GPIO Input Buffer Control Register
  6. 3Feature Differences for System Consideration
    1. 3.1 New Features in F28P55x
      1. 3.1.1 Programmable Gain Amplifier(PGA)
      2. 3.1.2 Universal Serial Bus (USB)
      3. 3.1.3 5V Failsafe IOs
      4. 3.1.4 Flash Write Protection
      5. 3.1.5 Neural-Network Processing Unit (NPU)
    2. 3.2 Communication Module Changes
    3. 3.3 Control Module Changes
    4. 3.4 Analog Module Differences
    5. 3.5 Other Device Changes
      1. 3.5.1 PLL
      2. 3.5.2 PIE Channel Mapping
      3. 3.5.3 Bootrom
      4. 3.5.4 SW Libraries Included in the ROM
      5. 3.5.5 AGPIO
    6. 3.6 Power Management
      1. 3.6.1 LDO/VREG
      2. 3.6.2 POR/BOR
      3. 3.6.3 Power Consumption
    7. 3.7 Memory Module Changes
    8. 3.8 GPIO Multiplexing Changes
    9. 3.9 Analog Multiplexing Changes
  7. 4Application Code Migration From F28003x to F28P55x
    1. 4.1 C2000Ware Header Files
    2. 4.2 Linker Command Files
    3. 4.3 C2000Ware Examples
  8. 5Specific Use Cases Related to F28P55x New Features
    1. 5.1 PGA
    2. 5.2 USB
  9. 6EABI Support
    1. 6.1 Flash API
  10. 7References
  11. 8Revision History

PCB Hardware Changes for the 100-Pin PZ, 80-Pin PNA and 64-Pin PM Packages

This section describes the F28003x and F28P55x differences that exist between the 100-Pin PZ, 80-Pin PNA and 64-Pin PZ packages.

100-Pin PZ: There are increased mux options on many analog pins on the F28P55x vs the F28003x. There is an additional 2 GPIOs on F28P55x that replace 2 power pins on the F28003x. Figure 2-1 outlines the differences.

80-Pin PN/PNA: There are increased mux options on many analog pins on the F28P55x vs the F28003x. There are an additional 2 GPIOs on F28P55x that replace 2 power pins on the F28003x. There is one less GPIO on the F28P55x due to the VREGENZ pin. Please note that the package pitch is changed with the F28003x having a 0.5mm pin pitch and the F28P55x having a 0.4mm pin pitch. Figure 2-2 outline the differences.

64-Pin PM: There are increased mux options on many analog pins on the F28P55x vs the F28003x. There is an additional 2 GPIOs on F28P55x that replace 2 power pins on the F28003x. There is one less GPIO on the F28P55x vs the F28003x Q100 variant due to the VREGENZ pin. Figure 2-3 outlines the differences.

 100-Pin PT, F28003x and F28P55x
          Pin-Overlay Figure 2-1 100-Pin PT, F28003x and F28P55x Pin-Overlay
 80-Pin PN/PNA, F28003x and F28P55x
          Pin-Overlay Figure 2-2 80-Pin PN/PNA, F28003x and F28P55x Pin-Overlay
 64-Pin PM All Variants, F28003x and
          F28P55x Pin-Overlay Figure 2-3 64-Pin PM All Variants, F28003x and F28P55x Pin-Overlay