SPRUJ63A September 2022 – October 2023
The PCIe reference clock to the SoC is provided by the PCIe slot connector when the processor is configured as downstream port. PCIe reference clock from the SoC (SERDES0_REFCLK0) is provided to the PCIe slot connector during root complex mode of operation.