SPRUJ66A February 2023 – December 2023
AM62A Low Power SK EVM has a 40 pin test automation header (FH12A-40S-0.5SH) to allow an external controller to manipulate some basic operations like Power Down, POR, Warm Reset, Boot Mode control etc.
The Test Automation Circuit is powered by the 3.3V supply generated by a dedicated Always On regulator Mfr.Part# TPS62177DQCR. The SOC’s I2C1 instance is connected to the test automation header. Another I2C instance (BOOTMODE_I2C) from the Test Automation Header is connected to the 24 bit I2C boot mode IO Expander of Mfr. Part# TCA6424ARGJR to allow control of the boot modes for the AM62A SOC.
The test automation circuit has voltage translation circuits so that the controller is isolated from the IO voltages used by the AM62A. Boot mode for the AM62A can be user controlled by either using DIP Switches or the test automation header through the I2C IO Expander. Boot Mode Buffers are used to isolate the Boot Mode controls driven through DIP Switches or I2C IO Expander. The boot mode can be set using two 8-bit DIP switches on the board, which will connect a pull-up resistor to the output of a buffer when the switch is set to the ON position and to a weaker pull-down resistor when set to the OFF position. The output of the buffer is connected to the boot mode pins on the AM62A SOC and the output is enabled when the boot mode is needed during a reset cycle.
When boot mode is set through Test Automation header, the required switch values are set at the I2C IO expander output, which overwrites the DIP switch values to give the desired boot values to the SOC. The pins used for boot mode also have other functions which are automatically isolated by disabling the boot mode buffer during normal operation.
The power down signal from the Test automation header instructs the SKEVM to power down all the rails except for dedicated power supplies on the board. Similarly PORZn signal provides a hard reset to the SOC and WARM_RESETn for a warm reset to the SOC.
Pin no. | Signal | IO Direction | Pin no. | Signal | IO Direction |
1 | VCC3V3_TA | Power | 21 | NC | NA |
2 | VCC3V3_TA | Power | 22 | NC | NA |
3 | VCC3V3_TA | Power | 23 | NC | NA |
4 | NC | NA | 24 | NC | NA |
5 | NC | NA | 25 | DGND | Power |
6 | NC | NA | 26 | TEST_POWERDOWN | Input |
7 | DGND | Power | 27 | TEST_PORZn | Input |
8 | NC | NA | 28 | TEST_WARMRESETn | Input |
9 | NC | NA | 29 | NC | NA |
10 | NC | NA | 30 | TEST_GPIO1 | Input |
11 | NC | NA | 31 | TEST_GPIO2 | Bidirectional |
12 | NC | NA | 32 | TEST_GPIO3 | Input |
13 | NC | NA | 33 | TEST_GPIO4 | Input |
14 | NC | NA | 34 | DGND | Power |
15 | NC | NA | 35 | NC | NA |
16 | DGND | Power | 36 | SoC_I2C1_TA_SCL | Bidirectional |
17 | NC | NA | 37 | BOOTMODE_I2C_SCL | Bidirectional |
18 | NC | NA | 38 | SoC_I2C1_TA_SDA | Bidirectional |
19 | NC | NA | 39 | BOOTMODE_I2C_SDA | Bidirectional |
20 | NC | NA | 40 | DGND | Power |