The EVM supports three USB3.1 Gen1
Type A ports [J9][J11], which operate in Host mode. The combined VBUS output for
these ports is limited to 2.8A. Also supported is one USB3.1 Gen1 Type C interface
[J11], which can function as DFP. The VBUS output for this port is limited to 1.5A.
Note: TheUSB2.0 Micro-B connector [J4] is discussed in
Uart-over-USB section.
Note: The VBUS power capability assumes the selected input supply
is capable of supplying power for both SK-AM68 system and connected
peripherals.
Note: An example optional add-on USB Camera module for this
interface is the Logitech USB C270.
Note: The maximum length for the IO cables should not exceed 3
meters.