SPRUJ71 august 2023
The LAUNCHXL-F28P65X includes a TMS320F28P650DK9NMR device pre-programmed with a demo program. When the LaunchPad is powered on, the demo program begins with an LED blink sequence on LED4 and LED5. After a few seconds, the device switches into an ADC sampling mode.
Every 1 second, the ADC samples pin ADCINA4 and the sampled value is represented as follows: If the sample is above mid-scale (2048), the red LED4 illuminates. If the sample is below mid-scale, the green LED5 illuminates.
By default, the ADC is configured in external voltage reference mode. Thus, the shunt on J15 must be connected to make use of the on-board 3.0 V high-precision voltage reference device (REF6230). The mid-scale point occurs around 1.5 V. For more information about the analog voltage reference, see Section 3.1.11.
In addition to the LED indicators, ADC sample results are also displayed on your PC through the USB/UART connection. To view the UART information on your PC, first determine the COM port associated with the LaunchPad (see Figure 2-1). To do this in Windows, open the Device Manager. Look for an entry under Ports (COM & LPT) titled "XDS110 Class Application/User UART (COMX)", where X is a number. Remember this number for when you open a serial terminal.
The demo application's UART data was tested using PuTTY, which is a free and open-source terminal emulator. To view the UART data in a serial terminal program, open the COM port found using the Windows Device Manager with the following settings:
115200 Baud, 8 data bits, no parity, 1 stop bit.
After properly opening the serial port in your serial terminal, reset the LaunchPad by pressing the S1 reset button and observe the serial terminal to see the TI logo in ASCII art (see Figure 2-2).
After a few moments, the ADC value sampled on the ADCINA4 pin appears in the bottom right corner of the terminal and is updated each second (see Figure 2-3). Using a jumper wire, connect the ADCINA4 header to a 3.0 V, GND, or other 0-3.0 V signal to see the on-screen value change.