The software packages described in
Section 2.1 include
example projects that can be loaded and run on the F28P65x LaunchPad. If you
installed the C2000WARE software to the default installation path of
C:\ti\c2000\C2000Ware_<version>, you can find DriverLib-based
example applications in
C:\ti\c2000\C2000Ware_<version>\examples\f28p65x. The on-board
XDS110 is used with the On-Chip Flash Programmer tool to program applications to the
F28P65x LaunchPad.
Follow these steps to program example
applications onto the F28P65x LaunchPad development kit using the on-board XDS110
debug probe:
- Install Code Composer
Studio (CCS) IDE on a PC running Microsoft Windows.
- Connect the USB-A cable plug in
to an available USB port on the PC and plug the USB Type-C™ plug to the port
(USB1) on the F28P65x LaunchPad.
- Verify the following LEDs are
illuminated:
- LED1, at the top left of
the board, indicating 5 V USB power.
- LED7 indicating 3.3 V
power to the XDS110 debug probe.
- LED3 indicating 5.0 V power to the F28P650DK9 MCU.
- LED6 indicating 3.3 V
power to the F28P650DK9 MCU.
- Install Windows XDS110 and
Virtual COM Port drivers if prompted. Installation instructions can be found at
XDS110 Product Page.
- Run CCS IDE on the PC.
- Import a F28P65x project from
C2000WARE, or another installed software package, into the CCS IDE
workspace.
- Add the _LAUNCHXL_F28P65X
predefined symbol to the imported DriverLib example project for the software to
use relevant F28P65x LaunchPad signals.
- Open the projects
Properties → Expand the Build tab → Expand the C2000
Compiler tab → Select Predefined Symbol → Add
_LAUNCHXL_F28P65X pre-define NAME.
- Right click the project name and
select Rebuild Project in CCS IDE.
- Launch the LAUNCHXL-F28P65X
Target Configuration file and connect to the F28P65x device. Make sure that the
Target Configuration file is configured to use the 4-pin JTAG advanced
configuration. For additional details, see FAQ section.
- Click 'Load Program' and select
the program's binary to load. The binary is loaded onto the device and can now
be run and debugged.