SPRUJ79 November 2024 F29H850TU
FILE: wadi_ex1_duty_freq_capture.c
This example configures WADI1 Block 1 and Block 2 as follows
The WADI block has error status register that can be used to monitor if any erroneous signals occur. (BLKERRSTS)
This example also makes use of the Input X-BAR. GPIO0 (ePWM1A output) is routed to the input X-BAR, from which it is routed to WADI SIG1 input.