SPRUJ79 November 2024 F29H850TU
Multiple reset sources of ESCSS are combined to make the reset vector that drives the EtherCAT and companion devices (PHYs) on this MCU. The RESET_OUT is asserted only when configured to be a reset. If configured as an interrupt or NMI, the local host completes the reset.
By default, RESET_OUT performs no action and must be setup to cause the reset to the EtherCAT core and PHY. The input events to RESET_OUT include the remote EtherCAT MainDevice, local host application, and EtherCAT soft reset.
When the intent is to perform a reset to the ESCSS and the device, the following options are available to reset the device after software has given a reset to the ESCSS: