SPRUJ79 November 2024 F29H850TU
The RTDMA is connected through a slow access port, so all accesses take an extra cycle as opposed to the fast access port. For this reason, the RTDMA is enhanced to support local address generation within the EMIFSS arbiter initiator select 1 component. This enables read burst performance close to that of the fast access port, thereby improving throughput. For more information, refer to the Real-Time Direct Memory Access (RTDMA) chapter.