SPRUJ79 November 2024 F29H850TU
Figure 14-2 shows the connections between the EMIF and the internal requesters, along with the external EMIF pins. Section 14.2.2 contains a description of the entities internal to the MCU that can send requests to the EMIF, along with their prioritization. Section 14.2.3 describes the EMIF external pins and summarizes their purpose when interfacing with the SDRAM and asynchronous devices.