SPRUJ79A November 2024 – December 2025 F29H850TU , F29H859TU-Q1
Distributed clocks (DC) allows the tracked time at ESC be synchronized across the EtherCAT network, which makes precisely timed events possible throughout the network. Events can be realized with triggers from ESC outputs that are programmed to create a toggle at a certain absolute time tracked by the ESC or through sampling of timestamp of certain system event inputs to ESC that can further be used for synchronizing the time.