The Excel-based J721S2 Power Estimation tool allows users to estimate thermal power based on specified loadings for different components (compute cores and peripherals) of the system-on-chip (SoC). The tool allows the user to pre-populate the various fields (which components are used, and utilization of the major components) from a set of representative use cases. This gives a starting point from which a new use case can be customized to judge the power and loadings of their own use case. The tool provides a breakdown of thermal power at the junction temperature (Tj) entered, and also provides a table of power delivery network (PDN) currents computed for this defined use case at Tj = 125°C or 105°C. The J721S2 Power Estimation tool supports the SOCs (e.g. J721S2, TDA4VE, TDA4AL, TDA4VL, AM68) in the J721S2 family.
The tool gives two power estimates:
Download the tool described in this document from https://www.ti.com/lit/zip/SPRUJ91A.
All trademarks are the property of their respective owners.