The Excel-based J721S2 Power Estimation tool allows users to estimate thermal power based on specified loadings for different components (compute cores and peripherals) of the system-on-chip (SoC). The tool allows the user to pre-populate the various fields (which components are used, and utilization of the major components) from a set of representative use cases. This gives a starting point from which a new use case can be customized to judge the power and loadings of their own use case. The tool provides a breakdown of thermal power at the junction temperature (Tj) entered, and also provides a table of power delivery network (PDN) currents computed for this defined use case at Tj = 125°C or 105°C. The J721S2 Power Estimation tool supports the SOCs (e.g. J721S2, TDA4VE, TDA4AL, TDA4VL, AM68) in the J721S2 family.
The tool gives two power estimates:
Download the tool described in this document from https://www.ti.com/lit/zip/SPRUJ91A.
All trademarks are the property of their respective owners.
The SoC power is typically considered to have two different components – dynamic power and leakage.
The dynamic power is computed based upon two numbers for the IP – max power and idle power (both scaled to the voltage). The dynamic power is computed as the weighted average of the max and idle power:
The leakage power is computed based on voltage, junction temperature, and manufacturing process variation. While the process and voltage have strong effects on the leakage power, the leakage power increases exponentially with Tj