SPRUJ91A april   2023  – may 2023 AM68 , AM68 , AM68A , AM68A , TDA4AL-Q1 , TDA4AL-Q1 , TDA4VE-Q1 , TDA4VE-Q1 , TDA4VL-Q1 , TDA4VL-Q1

 

  1.   1
  2.   Abstract
  3.   Trademarks
  4. 1Contributions to Power
  5. 2How to Use the Tool
  6. 3Use Case
    1. 3.1 Core Processor Utilization
    2. 3.2 Key IP Frequency Selection
    3. 3.3 Memory Interfaces
    4. 3.4 PHYs
    5. 3.5 High Speed Serial Interface
    6. 3.6 Environmental
    7. 3.7 LVCMOS IOs
    8. 3.8 Buttons
    9. 3.9 Starting Use Case
  7. 4Results Sheet
    1. 4.1 Thermal Power Estimate
    2. 4.2 Peak / PDN Power Estimate
  8. 5Three Specific Pre-Loaded Use Case Results
    1. 5.1 ARM Only
    2. 5.2 Superset
    3. 5.3 Valet Park
  9. 6Summary of Power for Pre-Populated Use Cases
  10. 7Revision History

PHYs

The J721S2 device family has several PHYs; for the PHYs with multiple instances, in addition to the mode and the utilization, the user can also select how many of the instances are used:

  • 2x Camera Stream Interface (CSI) 2.0 Receive PHYs each with 4 Lanes
  • 2x CSI2.0 Transmit PHYs each with 4 Lanes
  • Multi Media Card Interface (MMC) for eMMC only
  • 2x Display Subsystem Display Serial Interface (DSI) Transmit interface (using the CSI2.0 Tx PHY)
  • Universal Serial Bus (USB) 2.0 PHY

GUID-20230330-SS0I-2GKK-GXV0-CKSGQ3X6S0CG-low.png