Note: Voltage Domains, Power Domains, and Local Power Sleep
Controllers – In the Environmental section of the Use Case tab, the user selects the
voltage for configurable voltage domains. Within a voltage domain (e.g.
VDD_CPU_AVS), some circuitry is placed within a power domain (e.g. C7x_0 and MMA are
within PD_C7_0); the power domain can break the connection to the voltage domain
if-and-only-if all of the IP within the power domain is unused. Circuitry within an
off power domain, do not contribute power – leakage or dynamic – to the power
budget. Within the power domain, IP is controlled by a local power sleep controller
(LPSC) which controls the clock and reset to the IP. IP which is not clocked does
not contribute dynamic power to the overall device power, but contributes leakage
power unless the IP resides in an unpowered power domain.
Note that a voltage domain
typically has some IP that is within a power domain and other IP that is not
within a power domain.