SPRUJ93 august 2023
The AM263x Control Card features a High Security, Field Securable (HS-FS) device. An HS-FS device has the ability to use a one time programming to convert the device from HS-FS to High Security, Security Enforced (HS-SE).
The AM263x device leaves the TI factory in an HS-FS state where customer keys are not programmed and has the following attributes:
The One Time Programmable (OTP) keyrwriter converts the secure device from HS-FS to HS-SE. The OTP keywriter programs customer keys into the device eFustes to enforce secure boot and establish a root of trust. The secure boot requires an image to be encrypted (optional) and signed using customer keys, which is verified by the SoC. A secure device in the HS-SE state has the following attributes: