Figure 3-10 shows the
reset architecture of the AM263x Control Card.
The AM263x SoC has the following
resets:
- PORz is the Power-On-Reset
for the MAIN Domain.
- WARMRESETn is the Warm Reset
to MAIN Domain.
The PORz signal is driven by a 3-input
AND gate that generates a power on reset for the MAIN domain when:
- The PMIC drives the NRES, MCU
Reset output signal low.
- The Voltage Monitor
(TPS37042A3OFDDFRQ1) drives either RESET1 or RESET2 when VSYS_3V3A or
VSYS_1V2 respectively are outside of the defined boundaries. For VSYS_3V3A,
RESET1 is asserted when SENSE1 is either 8% above or below 3.3 V (including
device accuracy). For VSYS_1V2, RESET2 is asserted when SENSE2 is either 5%
above or below 1.2 V (including device accuracy.
- The user push button (SW2) is
pressed.
- The Test Automation Header
outputs a logic LOW signal (TA_PORZn) to a P-Channel MOSFET gate which
causes V_GS of the PMOS to be less than zero and so the PORz signal connects
to the PMOS drain which is tied directly to ground.
The PORz signal is tied to:
- AM263x SoC PORz input
- RGMII1 Ethernet PHY
reset
- ICSSM1 Gigabit Ethernet PHY
reset
- ICSSM2 Industrial Ethernet
PHY reset
- BOOTMODE buffer output
enable
The WARMRESETn signal creates a warm
reset to the MAIN domain when:
- The user push button (SW4) is
pressed.
- The Test Automation Header
outputs a logic LOW signal (TA_RESETz) to a P-Channel MOSFET gate which
causes V_GS of the PMOS to be less than zero and so the RESETz signal
connects to the PMOS drain which is tied directly to ground.
The WARMRESETn signal is tied to:
- AM263x SoC WARMRESETN
output
- RESETz signal created from
push button + PMOS logic
- IO Expander reset
- Micro SD reset
The AM263x Control Card also has an
external interrupt to the SoC, INTn, that occurs when:
- The user push button (SW1) is
pressed.
- The Test Automation Header
outputs a logic LOW signal (TA_GPIO1) to a P-Channel MOSFET gate which
causes V_GS of the PMOS to be less than zero, connecting the INTn signal to
he PMOS drain tied directly to ground.