For assembly of the J7EXPA01EVM add-on module with
the J721EXCPXEVM and J784S4XEVM systems, follow the instructions and illustration
below.
- If assembling with previously used base EVM, then
make sure all power cables and other accessory cables are removed. The EVM must
be configured similar to as originally delivered.
- Orient the EVM such that the processor is facing
downward. The expansion connectors of the EVM must be facing upward.
- Remove the four stand-offs in the area of
expansion connector to the washer, leaving the threaded stand-off still
attached.
- Install the J7EXPA01EVM module by aligning the
mounting holes and mating connectors. Press firmly to make sure the connectors
are seated.
- Re-install the four removed stand-offs, but
without the thin washer.
Note: The washer is to help level
the board accounting for an expansion board PCB thickness.