SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The DPI FIFO is used to buffer all the active pixel data from the DPI interface during the active line. The depth of the FIFO must be selected to allow the pixel to be stored after the DPHY request to ready delay is introduced at the start of every frame. The FIFO will fill to a depth based on the tx_byte clock cycles used from the point where VSYNC is identified to the response from the DPHY link after it has exited Low Power and entered the zeroes state on the active data lanes.
Figure 12-550 presents DPI interface to DSI DPHY timing diagram.
The timing diagram above illustrates how the packets are generated for a DPHY with two and with four lanes activated. The diagram shows that the tx_byte clock changes based on the number of lanes, and that the configuration register values for the number of bytes used for HSA, HBP and HFP will remain the same.
The register values calculated for each of the line synchronization stages needs to take the number of bytes used to form the packet into account so that the timing for each stage aligns to the timing of the DPI input and most importantly that the total number of bytes exactly matches the number of byte clock cycles. The values used for the Horizontal Front porch must be larger than the combined horizontal sync and back porch to allow the DPI FIFO to empty.
The basic rule is that the values used for the DSI will be based on the DPI × BPP/8.
The DPI graphics driver must be configured with horizontal values that can be directly translated to DSI packet payloads.
These values will then form the number of tx_byte_clk cycles used to send the bytes over the number of active lanes. So, for an RGB888, DSI configuration the minimum values will be:
The diagram below, D-PHY Timings Control (see Figure 12-551), illustrates the byte mapping for a four lane DPHY link. In this example, the calculation for the horizontal sync stage aligns exactly across the four byte lanes.
The next stage is the horizontal back porch:
The value used in the HBP count can be used to account for the Header bytes used in the active data packet in next stage, although it is best to add this to the HFP stage calculation and allow time to empty the FIFO.
The Active part of the line will be a fixed size based on the line size and BPP, and include the six bytes for the packet header and CRC. The final stage is the horizontal front porch.
The HFP value should be adjusted to ensure that the number of tx_byte clock cycles for the horizontal line exactly matches the pixel clock cycles for the line times the BPP.
The timing diagram below, Control Block, illustrates the byte alignment changing when the HBP calculated is two bytes shorter than the previous case. This leads to the active and front porch packet headers beginning two bytes earlier, however the HFP count is adjusted to keep the end of the line on exactly the same tx_byte_clk cycle count.
The recommendation is to ensure that the total bytes for each horizontal line results in an exact integer tx_byte clock cycles (Total_bytes MOD num_of_lanes = zero), except for the case where the clocks are not exactly matched.