SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
The MCSPI controller has a built-in 64-byte buffer to unload the DMA or interrupt handler and improve data throughput.
This buffer can be used by only one channel at a time and is selected by setting the MCSPI_CHiCONF[28] FFER or MCSPI_CHiCONF[27] FFEW bit to 1. If several channels are selected and several FIFO enable bit fields are set to 1, the controller forces the buffer not to be used; the driver must set only one FIFO enable bit field.
The buffer can be used in the following modes:
Every word length (MCSPI_CHiCONF[11-7] WL) is supported.
In transmit-and-receive mode, the buffer can be used in transmit (see Figure 12-43) or receive (see Figure 12-44) directions, or in both directions. If only one direction is chosen in transmit-and-receive mode, the full buffer is used for this direction. In both directions, the buffer is split into two halves, one for each direction (see Figure 12-45).
Two levels (MCSPI_XFERLEVEL[5-0] AEL and MCSPI_XFERLEVEL[13-8] AFL) rule the buffer management. The granularity of these levels is 1 byte; it is not aligned with the MCSPI word length. The driver must set these values as a multiple of the MCSPI word length defined in WL. Table 12-22 lists the number of bytes written in the FIFO, depending on the word length.
MCSPI Word Length (WL) | |||
---|---|---|---|
3 ≤ WL≤ 7 | 8 ≤ WL ≤ 15 | 16 ≤ WL ≤ 31 | |
Number of bytes written in the FIFO | 1 byte | 2 bytes | 4 bytes |
The FIFO buffer pointers are reset when the corresponding channel is enabled or the FIFO configuration changes.