SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
Setting the pause bit in the Channel N Control Register (<BCHANRT[a]_TRT_CTL> [29] TX_PAUSE]) will suspend the channel from arbitration resulting in a halting of the flow of data. Clearing this bit will cause the channel to be added back into the arbitration list. Pausing a channel has no other destructive side effects (other than potentially overflowing trigger events.