SPRUJB3 March 2024 AM67 , AM67A , TDA4AEN-Q1 , TDA4VEN-Q1
AASRC mode is similar to X-Y FIFO mode, the static TR consists of the following information:
Param | PSIL Addr | Field | Description |
---|---|---|---|
Burst | 0x400 | 31 | Not used |
Acc32 | 0x400 | 30 | When set, enables 32-bit access mode. On a 32-bit PDMA, all accesses will have XCNT=4 to support legacy IP that is not fully VBUSP compliant. This bit is ignored if the PDMA VBUSP port is not 32 bits wide. |
X | 0x400 | 26:24 | Element size. This field specifies how much data is transferred in each write which is performed by the DMA. This field is encoded as follows: 0 = 8 bits, 1 = 16 bits, 2 = 24 bits, 3 = 32 bits, and 4-7 = RESERVED |
Y | 0x400 | 11:0 | FIFO element count. In AASRC mode, a channel can service multiple FIFOs using a list supplied in its FIFO configuration. This field specifies how many times to service the FIFO list, hence how many elements to transfer to each FIFO, each time a trigger is received on the channel. Note for each loop specified by the value of Y, the entire list is processed. For example, if the FIFO list is 0, 1, 2, 3, and Y is set to 2 loops, the FIFOs are serviced in the order: 0, 1, 2, 3, 0, 1, 2, 3. |
Z | 0x401 | 23:0 | Not used |