SPRUJC5 April 2024 TMS320F28P550SJ , TMS320F28P559SJ-Q1
Verifies region specified is erased value.
Fapi_StatusType Fapi_doBlankCheck(
uint32 *pu32StartAddress,
uint32 u32Length,
Fapi_FlashStatusWordType *poFlashStatusWord
)
pu32StartAddress [in] | Start address for region to blank check |
u32Length [in] | Length of region in 32-bit words to blank check |
poFlashStatusWord [out] | Returns the status of the operation if result is not Fapi_Status_Success |
->au32StatusWord[0] | Address of first non-blank location |
->au32StatusWord[1] | Data read at first non-blank location |
->au32StatusWord[2 | Value of compare data (always 0xFFFFFFFF) |
->au32StatusWord[3] | N/A |
This function checks if the flash is blank (erased state) starting at the specified address for the length of 32-bit words specified. If a non-blank location is found, corresponding address and data will be returned in the poFlashStatusWord parameter.
None